Communication and Rapid Shutdown (RSD) Connections
To make communication connections:
Remove the cover over the battery's "To Inverter" port and then connect a 600 V CAT5e cable from the Schneider Inverter's port to the battery's "To Inverter" port.
- For dual battery systems, install a CAT5e cable from Battery 1's OUT port to Battery 2's IN port.
- For triple battery systems, daisy-chain a CAT5e cable from Battery 1's OUT port to Battery 2's IN port, and from Battery 2's OUT port to Battery 3's IN port.
1 |
Threaded lock nut |
2 |
Grey silicone ring |
3 |
Black silicone ring |
4 |
Connector plug housing |
Type |
Required specifications |
Example |
---|---|---|
Communication cable |
|
BELDEN 7958A DataTuff® (or equivalent) For more information, see https://www.belden.com/ |
Note: For assembly information, follow instructions from the manufacturer. |
|
Pin Number |
Signal |
Description |
1 |
CAN_H |
CAN-High |
|
2 |
CAN_L |
CAN-Low |
|
3 |
GND |
Ground |
|
4 |
RSD+ |
Rapid Shutdown, positive |
|
5 |
RSD+ |
Rapid Shutdown, positive |
|
6 |
RSD- |
Rapid Shutdown, negative |
|
7 |
GND |
Ground |
|
8 |
RSD- |
Rapid Shutdown, negative |