Overview

Schneider Boost is a high voltage, Lithium Iron Phosphate (LFP) battery storage system. It includes an integrated Battery Management System (BMS), and battery disconnect switch. It is intended for residential applications including energy management and backup power. The Schneider Boost is required to be installed with the Schneider Inverter in all cases, and for backup power, a Schneider Electric compatible Backup Controller is also required. When installed together, the Schneider Boost and Schneider Inverter can be configured and monitored remotely, using the Schneider Installer Portal (qualified personnel) or Schneider Home mobile app (home owners).

Note:

  • When designing your system, ensure that only compatible part numbers are selected, as described in the Schneider Inverter and Boost manuals.

  • Obtain all necessary permits prior to starting the installation. Installations must meet all local codes and standards.

  • Before installing the Schneider Boost, check it over for any signs of shipping damage. If any damage is found, contact Technical Support.