FDM128 Icons

 

Icon List

Header Icons

Icon

Description

G-SE-0019686.2.gif-high.gif 

Go to General view menu

G-SE-0043125.1.gif-high.gif 

Refresh the display of the names of connected devices

G-SE-0038933.2_3.jpg 

Locate the device

G-SE-0038842.1.gif-high.gif 

Go to Login/Access Code settings menu

G-SE-0019685.2.gif-high.gif 

Go to Editing devices menu

G-SE-0019684.2.gif-high.gif 

Go to Communication settings menu

G-SE-0019687.2.gif-high.gif 

Go to General settings menu

Footer Icons

Icon

Description

G-SE-0019657.2.gif-high.gif 

Go to next screen

G-SE-0019658.2.gif-high.gif 

Go to previous screen

G-SE-0019659.1.gif-high.gif 

Switch to bargraph mode

G-SE-0019660.1.gif-high.gif 

Switch to numeric mode

G-SE-0019661.1.gif-high.gif 

Switch to dial mode

G-SE-0039107.1.gif-high.gif 

Switch to icon mode

G-SE-0038935.1.gif-high.gif 

Switch to list mode

G-SE-0038933.2_4.jpg 

Locate a circuit breaker

Action Icons

Icon

Description

G-SE-0019663.1.gif-high.gif 

Reset measurements displayed in the previous screen

G-SE-0038936.1.gif-high.gif 

Reset all measurements and counters of the circuit breaker

G-SE-0019662.1.gif-high.gif 

Reset circuit breaker

G-SE-0038933.2_5.jpg 

Locate a circuit breaker

G-SE-0019655.2.gif-high.gif 

Decrease level

G-SE-0019656.2.gif-high.gif 

Increase level

G-SE-0019653.1.gif-high.gif 

Display next tabs

G-SE-0019654.1.gif-high.gif 

Display previous tabs

Alarm Status Icons

Icon

Description

G-SE-0019681.1.gif-high.gif 

Circuit breaker status is OK

G-SE-0019680.1.gif-high.gif 

Circuit breaker is offline

G-SE-0019679.1.gif-high.gif 

Medium priority alarm is occurring

G-SE-0019677.2.gif-high.gif 

High priority alarm is occurring

Circuit Breakers Status Icons

Icon

Description

G-SE-0019664.2.gif-high.gif 

Circuit breaker is charged

G-SE-0019668.2.gif-high.gif 

Circuit breaker is discharged

G-SE-0019665.3.gif-high.gif 

Circuit breaker is closed

G-SE-0019672.3.gif-high.gif 

Circuit breaker is open

G-SE-0019666.2.gif-high.gif 

Withdrawable circuit breaker is connected

G-SE-0019669.2.gif-high.gif 

Withdrawable circuit breaker is disconnected

G-SE-0019673.1.gif-high.gif 

Capacitive load

G-SE-0019674.1.gif-high.gif 

Inductive load

G-SE-0019675.2.gif-high.gif 

Cradle position: Test active

G-SE-0019676.2.gif-high.gif 

Cradle position: Test disabled

G-SE-0053678.1.gif-high.gif 

Global health status (For MasterPact MTZ only)