1. Downloading the PME/EBO Integration Toolkit

The PME/EBO Integration Toolkit is used to integrate PME into Building Operation WorkStation.

Starting with PME 2021,

  • The Toolkit contains ETL only. To get the toolkit, download the PME_EBO Integration Tools.zip file from the Exchange Extranet (see Resources for link information). Extract the files in the zip archive to the location on the Building Operation server, where you want to run the tools.

  • The Building Operation components, snippets, and binding template are available in PME ISO under EBO Integration Files folder. Copy this folder to the location on the Building Operation server, where you want to run the tools.

  • The Integration Utility is a Web application settings in PME. Open the Settings page from the SETTINGS link in the Web Applications banner and navigate to Security -> Integrations-> Integration Utility.