Install the PME/EBO Integration solution

Installing the PME/EBO Integration solution includes the following steps:

  1. Downloading the PME/EBO Integration Toolkit
  2. Installing EcoStruxure Building Operation
  3. Installing the components, snippets, and binding template
  4. Installing PME
  5. Using PME EWS Client or Installing ETL (only for Architecture 1 solutions)

    NOTE: From PME 2022, EWS client is supported. Use PME EWS client for importing historical data from Building Operation to PME.

NOTE: Steps 1 - 4 are required for both solution architectures.

See the following sections for details.