Integration Limitations
Only the PME Standalone Architecture installation type, where the PME application server and the database server are installed on the same computer, is supported by this integration. The PME Distributed Database architecture installation type is not supported. See System architecture for more information on PME installation architectures.