Insulation Monitoring Module Design

The Insulation Monitoring Module provides monitoring for isolated (IT) power systems, such as the ones found in hospital operating rooms. It also helps in locating isolation faults. The module can be configured for applications based on the IEC standard, and for applications based on the ANSI standard.

Components

The following components are part of this module:

  • Insulation Monitoring Report
  • Vista diagrams
  • VIP framework
  • Insulation Monitoring Configuration Tool

Prerequisites

  • This module can only be used with specific device types, see Supported measurements and devices for more information.
  • The measurement data for the report must be available as historical data logs in the database.

Design Considerations

  • In IEC configuration, the module monitors insulation resistance.
  • In ANSI configuration, the module monitors total hazard current.
  • This module requires the configuration of VIP frameworks and Vista diagrams.
  • This module is used for very specific applications. It needs certain types of devices and equipment.

See Insulation Monitoring Design for ANSI for more information on this application in the ANSI market.

 

Related topics:

Insulation Monitoring Module topics

Other software features

Other Software Modules