Advanced Systems

An advanced system is defined by any of the following characteristics:

  • Custom measurement logging with <15-minute intervals
  • Custom applications using the VIP module
  • Power Quality Performance monitoring
  • Large number of concurrent users
  • High percentage of advanced level devices in the system
  • Large number of branch circuit monitor devices in the system
  • Large scale data exchange with third party systems (for example through OPC, ETL, or EWS)
  • Other resource intensive software systems installed on the same computer
  • Distributed Database architecture

Minimum recommended computer hardware for servers in Advanced Systems:

System Size Devices Users OPC Tags Computer Hardware RAM
Standalone architecture Distributed Database architecture - Application Server Distributed Database architecture - Database Server
Small ≤ 100 ≤ 15 5000
Workstation
Intel Xeon W-21xx (4 Core)*
16 GB 16 GB 16 GB
Medium ≤ 250 ≤ 20 10000
Server
Intel Xeon Bronze (8 core)*
24 GB 16 GB 24 GB
≤ 600 ≤ 35 30000
Server
Intel Xeon Silver (10 core)*
32 GB 24 GB 32 GB
Large ≤ 2500 ≤ 50 50000
Server
Intel Xeon Silver (12 core)*
64 GB 32 GB 64 GB

*Equivalent or higher processor