After updating the software

After installing a Cumulative Update (CU)

After you have installed a CU, do not simply use the Reconfigure function of the original installer of your PME software anymore.

To reconfigure the software, after installing CUs, you must run the Reconfigure function of the original installer first, and then run the Reconfigure function of each CU installer in sequential order. For example, if you have installed CU1 and CU2 on your system, you must run Reconfigure on the original PME installer, then Reconfigure on the CU1 installer, and then Reconfigure on the CU2 installer. See Reconfigure for information on this function.