Uploading Multiple Report Template (Report Pack)

You can upload multiple report template (Report Pack) at a time as a .zip file to use it along with other report templates.

To upload multiple report template (Report Pack):

  1. In Upload Report Template, select Report Pack(.zip).

    NOTE: Make sure that multiple report templates are zipped as a single .zip file.

  2. Click Select File to navigate to the location of the .zip file.
  3. Select the file and click Open.
  4. Click Upload.

    A progress bar displays the upload status.

    The uploaded report are unzipped and is in ...\ Power Monitoring Expert\web\ReportDepot\ION Reports\ION Report Packs

NOTE: After you uploaded the Report Template, you can access it, together with the default templates, in the Report Library.

For information on how to use the Upload Report Template, see: