Viewing previous change details
Manual Data Editor maintains an audit log which records all changes to logged data made by the tool. The log is filtered by source/measurement.
To view previous change details:
- In Manual Data Editor, click Load New Data to open the Load Data dialog box.
NOTE: Load Data opens automatically when you start Manual Data Editor.
- In Load Data:
- Select the Source for which you want to see the audit log.
- Select the Measurement for which you want to see the audit log.
- Click Add Data to Selection to add the source/measurement to the list of items to be opened in the data editor.
- (Optional) Repeat step 2 to add additional sources and measurements to the selection list.
- Click Load Data to open the source/measurement data entry fields in the data editor.
NOTE: Ignore the settings for Time Range and Options, they have no influence on the display of the audit log.
- (Optional) In the data editor, click Load New Data to change which data is loaded, the time range, or the editor options.
- Click View Log to open the audit log for these sources/measurements.
- View the audit log.
- Close Manual Data Editor.
For information on how to use the Manual Data Editor , see:
- Editing existing logged measurement data
- Adding manually collected measurement data
- Viewing previous change details
- Reverting previous data edits
- Creating new measurements
For reference information see: