Insulation Monitoring Hardware Configuration for IEC
This section contains information about the hardware devices used in an insulation monitoring solution. Refer to the installation manuals for each device for instructions, safety messages, and parameter details.
warning
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
NOTE:
- Isolated power panels, optional monitoring devices, and communications for hardware must be installed in the designated areas.
- The insulation monitoring device must be configured correctly, and time synced to the EGX gateway.