Configure Power Quality Analysis Report

The Power Quality Analysis Report does not need configuration to work, unless you want to include output for the Power Factor section in the report.

The Power Factor section reports the power factor information for the incomer meters in the system. The report retrieves the incomer meter definition from the Power Quality Group definition. See for more information on how to define the incomer meters.

Alternatively, the Power Factor section can be toggled off when generating the report.