Editing the generator Evaluation Method

Use the Evaluation Method editor to select the evaluation method and the decision criteria for the Pass/Fail assessment of a generator test.

To edit the Evaluation Method:

  1. Click Edit Evaluation Method to open the evaluation method editor.
  2. Complete the following fields:
    • Evaluation Method - Select an evaluation method. Define the evaluation criteria.

      NOTE: Different evaluation criteria are displayed depending on which evaluation method is selected. See the table below for details.

  3. Click OK to save the configuration and close the Edit Evaluation Method window.

The following table shows the evaluation methods and their respective pass/fail criteria:

Evaluation Method Pass/Fail Criteria
Load (= Default) To Pass, the generator must run at the Suggested Load %(*) for the Run Duration (Minutes).
Engine Temperature To Pass, the generator must run at or above the Minimum Engine Temperature °C/°F for the Run Duration (Minutes).
Exhaust Gas Temperature To Pass, the generator must run at or above the Minimum Exhaust Gas Temperature °C/°F for the Run Duration (Minutes).
Load Bank To Pass, the generator must pass the selected stages consecutively. For each stage, it must run at the Suggested Load %(*) for the Run Duration (Minutes).
Load OR Engine Temperature To Pass, the generator must pass either the Load or the Engine Temperature test.
Load OR Exhaust Gas Temperature To Pass, the generator must pass either the Load or the Exhaust Gas Temperature test.
Load AND Exhaust Gas Temperature To Pass, the generator must pass either the Load and the Exhaust Gas Temperature test.
Load AND Engine Temperature To Pass, the generator must pass either the Load and the Engine Temperature test.
Load OR Engine Temperature OR Exhaust Gas Temperature To Pass, the generator must pass either the Load, or the Engine Temperature, or the Exhaust Gas Temperature test.
Load OR Engine Temperature AND Exhaust Gas Temperature To Pass, the generator must pass either the Load test, or the Engine Temperature and the Exhaust Gas Temperature test.
Load AND Engine Temperature OR Exhaust Gas Temperature To Pass, the generator must pass both the Load and the Engine Temperature test, or the Exhaust Gas Temperature test.
Load AND Engine Temperature AND Exhaust Gas Temperature To Pass, the generator must pass the Load and the Engine Temperature test and the Exhaust Gas Temperature test.

(*) The Suggested Load % is based on the generator nameplate rating.

The following table shows the default test criteria for each evaluation method:

NOTE: Update these values to meet the regulations mandated by your local jurisdictions, or to meet the manufacturer recommendations.

Test Name Stage Minimum Run Duration
Load n/a 30 % 30 minutes
Engine Temperature n/a 900 °C/°F 30 minutes
Exhaust Gas Temperature n/a 900 °C/°F 30 minutes
Load Bank 1 25 % 30 minutes
Load Bank 2 50 % 30 minutes
Load Bank 3 75 % 60 minutes