Moving or resizing a gadget on a dashboard
You can move or resize a gadget on a dashboard when the dashboard is in edit mode.
Moving a gadget
- Right-click a dashboard name in the Dashboard Library, then click Edit in the menu.
-
Position the mouse pointer in the title area of the gadget that you want to move.
The pointer changes to the Move shape (an image with 4 arrows).
-
Drag and drop the gadget to another position on the dashboard.
Other gadgets on the dashboard are re-positioned if additional space is required.
- Click Finish in Dashboard Controls to save your change.
Resizing a gadget
- Right-click a dashboard name in the Dashboard Library, then click Edit in the menu.
-
Position the mouse pointer at the lower right corner of the gadget.
A small triangular shape indicates that you can drag the corner.
-
Drag the corner to increase or reduce the size of the gadget.
Other gadgets on the dashboard are re-positioned if additional space is required.
- Click Finish in Dashboard Controls to save your change.
Related topics:
- Adding a new dashboard
- Editing a dashboard
- Sharing a dashboard
- Moving a dashboard
- Deleting a dashboard
- Set default options for a dashboard
- Configuring a slideshow
Gadgets:
- Adding a gadget to a dashboard
- Editing a gadget
- Moving or resizing a gadget on a dashboard
For reference information see:
For information on how to use Dashboards, see Dashboards.