Moving a dashboard

Move dashboards to a different location in the Dashboard Library to make them easier to find or easier to manage.

To move a dashboard:

  1. In Dashboards, open the Dashboard Library and navigate to the dashboard you want to move.
    (Optional) Add a new folder by clicking Add Folder at the bottom of the library panel, or by clicking Add Folder in the Options menu at the top of the library.
  2. Right-click the dashboard name or click Options for this dashboard and select Move To.... This opens the Select Location window.
  3. In Select Location, select the location where you want to move this dashboard.
  4. Click OK to move the dashboard.

Related topics:

Dashboards:

Gadgets:

For information on how to use Dashboards, see Dashboards.