Set default options for a dashboard
NOTE: For each user, Set as my default supersedes Set as system default. For example, if a user with supervisor-level access sets a dashboard as the system default dashboard, and another user sets a different dashboard as their default dashboard, that user's default dashboard takes priority over the system default dashboard, but only for them.
To set the default options for a dashboard:
- In Dashboards, open the Dashboard Library and navigate to the dashboard you want to set as default.
- Right-click the dashboard name or click Options for this dashboard and select Set as default to open the Configure Default Item dialog.
- Turn on one or both of Set as my default and Set as system default.
- Click OK to save the modified Dashboard Settings.
Related topics:
Dashboards:
- Adding a new dashboard
- Editing a dashboard
- Sharing a dashboard
- Moving a dashboard
- Deleting a dashboard
- Set default options for a dashboard
- Configuring a slideshow
Gadgets:
For reference information see:
For information on how to use Dashboards, see Dashboards.