Configuring device replacement

Configure device replacement to select the last replacement date and the replacement period for the list of devices based on the processed measurements.

To configure device replacement using the Device Replacement user interface:

  1. In Device Replacement, select the Device Replacement tab.
  2. Select the row of the device you want to configure and then click Edit in this row. This opens the Edit Device dialog.
  3. In Edit Device, Select the Last Replacement Date and Period for Replacement (Months).

  4. Click OK.