Deleting an EWS Client

Delete an EWS client if it is no longer needed, for example if the EWS server connected to EWS client has been removed from service. You can delete one EWS client at a time using the EWS Client user interface.

NOTE: When an EWS client is deleted, the configuration and mapping is also deleted.

To delete an EWS Client using the EWS Client user interface:

  1. In EWS Client table, select the row of the EWS client for which you want to delete, and then click Delete in this row.
  2. In the confirmation dialog box, click Delete.

 

Related topics:

For specific information on mapping, see

For reference information see: