Authorized Hosts
Use the authorized hosts settings to define third-party web resources that are allowed to either embed (frame) the PME web applications, or to which the PME web applications can redirect requests.
To define a third-party web resource as a Hosts That Can Frame, add the Uniform Resource Locator (URL) of that resource to the list, for example https://localhost:446
.
NOTE: Add all the names (URLs) that might be used for a host, for example the server name, "localhost", the IP address, and so on.
To define a third-party web resource as Hosts That Can Be Redirected To, add the hostname (no protocol, no port number) of that resource to the list, for example localhost
.
NOTE: Reset Internet Information Services (IIS) on the PME server after updating the Authorized Hosts settings.
An example for an application that requires an entry in the Hosts That Can Frame list is the integration of PME with EcoStruxure Building Operation. As part of that integration, PME Web Applications are embedded in Building Operation. For this to work, the Building Operation server URL must be added to the list of hosts that can frame.