EWS Server

EcoStruxure Web Services (EWS) requires a unique set of credentials to connect to the data exchange service.

To configure the credentials:

  1. Click Change Credentials, or Set Credentials, if you are configuring this setting for the first time, to enable the input fields.
  2. Add a user name.
  3. Type the password for the user in the Password and Confirm Password entry fields.
  4. Strong password criteria: A password must have at least 8 characters and contain at least one character from each of the following:

    • uppercase letters
    • lowercase letters
    • numbers
    • special characters.
  5. Click Save to apply your changes or Discard to retain the existing credentials.

NOTE: The EWS Server setting is only visible if EWS is enabled. When EWS is disabled, the EWS Server setting is hidden.