Personal Preferences

Use the personal preferences settings to update or edit your user profile details, change your account password, set your personal localization preferences, define a custom start of day, and choose your personal theme color.

NOTE: Your personal localization settings overrule the system localization settings for your user account. By default, your personal localization settings are the same as the system localization settings. See System and personal localization settings for details on the behavior of these settings.

NOTE: Your personal localization settings also apply to the Vista and Designer applications.

NOTE: The profile details settings and change password option are only available for standard accounts. For Windows accounts, this information is managed through Windows.

NOTE: The profile details and account password are the same as the ones configured for your account with User Manager.

To change any of the personal preferences:

  1. Edit the fields or select the options you want from the drop-down lists.
  2. If the supervisor wants to change the password, the password must meet the strong password criteria.

    Strong password criteria: A password must have at least 8 characters and contain at least one character from each of the following:

    • uppercase letters
    • lowercase letters
    • numbers
    • special characters.

    By default, in Custom Day Settings, the time will be 12.00 AM. You can define any Custom Start of Day as required.

  3. Click Save to apply the changed settings.