Viewing events

View events to investigate system activities in PME or to troubleshoot unexpected system behavior.

To view events:

  1. In the alarm viewer, open an existing event view from the view library or add a new View.
  2. View the event Information displayed in the alarms display pane.
    (Optional) In the view Library, right-click the view name or click Options for this view and select Edit to open the view settings. You can also open the view settings by double-clicking the view name. Adjust the settings for View Type, Priority and Sources to customize the view if necessary. Save the modified view settings or click Cancel to discard the changes.

TIP: Double-clicking an event in the events display table opens the associated alarm.

Related topics:

For reference information see:

For information on how to configure Alarms, see Alarms configuration.