Viewing incidents

View incidents to investigate system issues, to analyze what happened during a power disturbance or to identify root causes.

To view incidents:

  1. In the alarm viewer, open an existing incident view from the view library or add a new View.
  2. View the incident information displayed in the alarms display pane.
    (Optional) In the view library, right-click the view name or click Options , and select Edit to open the view settings. You can also open the view settings by double-clicking the view name. Adjust the settings for View Type, Priority, State, Sources, and Categories to customize the view if necessary. Save the modified view settings or click Cancel to discard the changes.

Related topics:

For reference information see:

For information on how to configure Alarms, see Alarms configuration.