Viewing a timeline analysis

View a timeline analysis to investigate the sequence of events that occurred during a single incident, multiple incidents, or alarms.

To view a timeline analysis for an incident:

  1. In the alarm viewer, open an existing incident view from the view library or add a new View.
  2. Find the incident for which you want to view the analysis, and click Open Timeline Analysis to open the timeline window.
    (Optional) Edit the view settings for the timeline analysis and save the view for future reference.

To view a timeline analysis for multiple incidents:

  1. In the alarm viewer, open an existing Incident view from the view library or add a new View.
  2. Find and select the incidents for which you want to view the analysis.

    TIP: Use Ctrl+Click to select individual alarms, use Shift+click to select a block of alarms.

  3. From the in the Options menu at the top of the alarms display pane, select Open Timeline Analysis on selection.

To view a timeline analysis for an alarm:

  1. In the alarm viewer, open an existing alarm history view from the view library or add a new View.
  2. Find the alarm for which you want to view the analysis and click Open Details.
  3. In the alarm details window, click Timeline Analysis.

Related topics:

For reference information see:

For information on how to configure Alarms, see Alarms configuration.