Viewing waveforms

View waveforms to investigate power quality events and identify root causes of disturbances.

To view waveforms:

  1. In the alarm viewer, open an existing Incident history view or alarm history view from the view library or add a new View.
  2. Find the incident or alarm for which you want to view waveforms and click Details . You can also open Details by double-clicking the incident or alarm instance.
  3. In Details, click Waveforms.

    TIP: Click Open Representative Waveform to see the representative waveform for this Incident or alarm instance.

  4. View the waveforms associated with the incident or alarm instance.

    (Optional) Click Inspect a waveform to see more details and to analyze the waveform.

Related topics:

For reference information see:

For information on how to configure Alarms, see Alarms configuration.