Dashboard Slideshows

Use slideshows to create collections of dashboards that are displayed in sequence without user interaction. A slideshow displays each of its dashboards for a short period of time and then displays the next dashboard. When it reaches the end, it starts over again with the first dashboard. It continuously cycles through all its dashboards in this way. Slideshows are a good option for unattended, kiosk type displays. See Configuring a slideshow for more details.

Related topics:

For reference information see:

For information on how to configure Dashboards, see Dashboards configuration.