Energy Equivalency gadget
This gadget shows a single value that is equivalent to the aggregated consumption input data, over a selected time period. The value can be scaled to represent a consumption equivalent measurement, such as CO2 emissions or primary energy units. The information is shown as a numeric value with unit, a custom text, and a custom graphic.
Example:
For information about configuring the gadget, see Configuring Gadgets.