Table gadget
This gadget shows real-time data from devices in the system. The information is shown in table format.
Example:
TIP: The measurements can be arranged in rows or in columns. The real-time data aggregation can be defined and data values can be highlighted for the defined threshold.
NOTE: User authentication is required if the table gadget is used in the slideshow. See Using Table gadget in Slideshow for more information.
For information about configuring the gadget, see Configuring Gadgets.