Web Viewer gadget

This gadget shows a web page inside the gadget frame in the dashboard.

warning

potential compromise of System availability, integrity, and confidentiality

Use cybersecurity best practices to help prevent unauthorized access to the software.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

NOTE: When you configure the Web Viewer gadget to access a website, you should be careful that the website does not include hidden malware, viruses, or content that could compromise your web client computers. It is recommended that the target site specified in the gadget be secured with the SSL or TLS protocol (accessed via HTTPS).

 

Example:

For information about configuring the gadget, see Configuring Gadgets.