Breaker Aging diagrams

NOTE: These diagrams are part of the Breaker Performance Module. This Module requires a separate license. The module must be configured before the diagrams can be used.

The breaker aging diagrams show aging and wear related details for the breaker devices. There are three different types of diagrams: Group summary diagram, group details diagram, and switchboard details diagram.

Group Summary Diagram

The group summary diagram shows the group summary status and the number of breakers in the group, for each of the groups setup with the Breaker Configuration tool.

Example:

Group Details Diagrams

A group details diagram shows the switchboards that are part of the group and the breakers in each switchboard.

TIP: Click the group icon for a group in the groups summary page to open the respective group details page.

Example (shows details page for Group 1):

Switchboard Details Diagrams

A switchboard details diagram shows detailed information for each breaker in the switchboard.

TIP: Click the switchboard icon for a switchboard in the group details page to open the device details page.

Example (shows details for Panel A):

 

Related topics:

For information on how to configure Diagrams, see Diagrams and graphics configuration.