The Diagrams user interface

The Diagrams user interface consists of a diagram display pane and a Diagram Library pane.

Diagrams display pane

The diagram display pane shows the diagram selected in the Diagram Library. The system administrator can set a system default diagram that users see when they first log in.

Diagram Library

The Diagram Library contains all the diagrams that are configured in the system. Diagrams can be listed individually, or they can be organized within folders. The Devices diagram folder is a system folder that is automatically generated. It cannot be edited or deleted. You use the Diagram Library to select the diagram you want to view.

TIP: To hide the library, click the Hide Library icon ( or ) in the top right corner of the library. To show the library, click the Show Library icon ( or ) at the top of the library ribbon, or click anywhere in the minimized library ribbon.

Related topics:

For information on how to configure Diagrams, see Diagrams and graphics configuration.