Viewing meter events

You can view meter events in the diagrams, in a table format, using the Diagrams application.

NOTE: You cannot acknowledge alarms on the screens generated by the Diagrams application since control functions are not supported. To acknowledge alarms, click the ALARMS icon in the Web Applications component to open the Alarm Viewer.

  1. Click the meter icon to open its diagram, then click the link or tab that contains the Meter events button.
  2. Click the Meter events button to open a table showing the meter events.

    The meter events table displays today's data by default.

    When the meter events table opens, 30 rows of data are displayed initially. As you scroll or page down, 30 additional rows of data at a time are added to the table.

  3. Click Change Date Range to change the timeframe for the data and select one of the available options for the data that you want to view. To specify a custom date range, select Between these dates then click the calendar icons to set a start and end date.

    If you select a custom date range, a maximum of 6000 rows of data are displayed. If the custom date range includes more than 6000 rows of data, you can display the additional records in increments of 30 rows at a time by scrolling down or pressing End.

Related topics:

For information on how to configure Diagrams, see Diagrams and graphics configuration.