Generator Activity Report

NOTE: This report is part of the Backup Power Module. This module requires a separate license.

Summary

The Generator Activity Report shows run information for backup generators, such as run times, durations, run reason, and overall run hours. Use this report to understand and manage your backup generator operation.

Details

The Generator Activity Report shows:

  • The number of non-emergency running hours as an annual total.
  • Running hours broken out into categories for Test, Power Outage, Load Shedding.
  • Bar graphs for generators with the number of hours of non-emergency run time.
  • A table with non-emergency and emergency run hours for each generator.
Prerequisites
  • The Backup Power Module must be configured.
  • The measurement data must be available as historical data logs in the database.
Report inputs:
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.