Generator Test EPSS Report

NOTE: This report is part of the Backup Power Module. This module requires a separate license.

Summary

The Generator Test EPSS Report shows load measurements and the sequence of events for generator test runs. You can configure it to meet the requirements of an Emergency Power Supply System (EPSS) test, including Automatic Transfer Switches (ATS). Use this report to assess the performance of your backup generation systems during test runs. You can also use this report to evaluate pass/fail criteria for EPSS testing.

NOTE: Emergency Power Supply System (EPSS) is a North American term used in the healthcare segment. It describes an arrangement of generators and automatic transfer switches, designed to provide backup power in case of a utility power interruption.

Prerequisites
  • The Backup Power Module must be configured.
  • The measurement data must be available as historical data logs in the database.
Report inputs:
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.