UPS Auto Test Report

NOTE: This report is part of the Backup Power Module. This module requires a separate license.

Summary

The UPS Auto Test Report shows test information for UPS systems, such as test times, pass/fail evaluation, and event logs. Use this report to assess the performance of your UPS systems during test runs.

NOTE: You can only use this report with certain types of UPS systems. See Backup Power Module configuration for details.

Prerequisites
  • The Backup Power Module must be configured.
  • The measurement data must be available as historical data logs in the database.
Report inputs:
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.