Billing Reports

NOTE: These reports are part of the Energy Billing Module. This module requires a separate license.

PME includes the following billing report templates:

CAUTION

inaccurate data results

Do not incorrectly configure the software or the devices.
Do not base your maintenance or service actions solely on messages and information displayed by the software.
Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.

Failure to follow these instructions can result in injury or equipment damage.

 

For information about changing the unit cost values in a rate file used for billing reports, see the Rate Editor tool.