Data Export - Extended
Summary

The Data Export - Extended Report gives logged measurement data in CSV file format. Use this report to import and analyze data in a third-party application, such as Microsoft Excel.

NOTE: This report has more details than the Data Export - Standard Report, but it supports a smaller data set.

Details

The data is organized in columns labeled Timestamp UTC, Timestamp, Value, Source, Measurement, and Unit. This makes it easier to create an Excel pivot table for analyzing the data in the file. The data is listed for each source and measurement by date and in the specified time segments for the data. This report can export 80 source measurements for 10 months.

Prerequisites
  • The measurement data must be available as historical data logs in the database.
Report inputs
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.