System Configuration Report
Summary
The System Configuration Report shows details about the monitoring devices in your network, including communications information. Use this report for device and communications network inventory and planning.
Prerequisites
- None
Report inputs
Type a title for the report in the text box.
Click Yes to include data warnings in the report. If there are none, the section is not included. Click No to exclude this section.
Example:
NOTE: This example only shows selected content from the report, it does not show the entire report.