Tabular Report
Summary

The Tabular Report gives logged measurement data in tabular format. Use this report to analyze logged data.

Details

You can create a report with multiple measurements from multiple sources. You can also select the option to include duplicate data in the report. This data can then be exported for use in another program, such as Microsoft Excel. If you want to only export your data to an Excel file, use the Data Export - Extended report or the Data Export - Standard report.

NOTE: The Tabular Report is limited to 30 source-measurement pairs. Multiple reports are required if the number of source-measurement pairs exceeds 30. Alternatively, consider using the Data Export - Standard report or the Data Export Extended report to generate a CSV file containing the data for the selected sources and measurements.

The generated report contains the following information: source; measurement; timestamp; and values.

Prerequisites
  • The measurement data must be available as historical data logs in the database.
Report inputs
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.