Continuous Thermal Monitoring Report
Summary

The Continuous Thermal Monitoring Report shows the status of the thermal monitoring system. The thermal monitoring system includes Low Voltage Switchboards, Medium Voltage substations, and Low Voltage Busways, which are equipped with temperature and environmental sensors. The report shows the alarm status, communication error, and normal data points information. Use this report to understand and manage the thermal monitoring system status.

Prerequisites

The thermal monitoring system must be connected to PME. See Thermal Monitoring of Low Voltage (LV) Busways and Thermal Monitoring of Medium Voltage (MV) Substations for more information.

Report inputs
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.