Insulation Monitoring Report (IEC)

NOTE: This report is part of the Insulation Monitoring Module. This Module requires a separate license.

Summary

The Insulation Monitoring (IEC) Report shows resistance, transformer load, relevant event log entries, and logged insulation related measurements, over the reporting period. Use this report to analyze and report on the insulation status of your ungrounded IT power system.

Details

The report includes:

  • An impedance graph, showing a comparison of impedance measurements to the impedance threshold.
  • A transformer load graph, showing a comparison of transformer load measurements to the load threshold.
  • An events table, showing information for each event that occurred in the reporting range.
  • A data log table, showing measurements for impedance, load, and temperature.
Prerequisites
  • The Insulation Monitoring Module must be configured.
  • The measurement data must be available as historical data logs in the database.

Report inputs

Hospital Operating Room Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.