IT Billing Reports
NOTE: These reports are part of the Energy Billing Module. This module requires a separate license.
PME includes the following IT billing report templates:
CAUTION
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
Failure to follow these instructions can result in injury or equipment damage.