UPS Power Report

NOTE: This report is part of the Capacity Management Module. This Module requires a separate license.

Summary

The UPS Power Report shows system loading compared to UPS backup power rating and redundancy design limits. Use this report for backup power system capacity analysis and planning.

Prerequisites
  • The Capacity Management Module must be configured.
  • The measurement data must be available as historical data logs in the database.
Report inputs:
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.