Trend Report
Summary

The Trend Report shows logged measurement data for multiple loads as a trend plot on the same axis. Use this report to compare different loads.

Details

NOTE: The Trend Report is limited to 30 source-measurement pairs. Multiple reports are required if the number of source-measurement pairs exceeds 30.

NOTE: The Trend Report was upgraded in Power Monitoring Expert 7.2.1 to include two new parameters: Include Data Table and Include Duplicates.

Trend Reports with subscriptions created prior to version 7.2.1 need to be updated and saved with the new parameters. To update a Trend Report:

  • Open each saved Trend Report. The new parameters are visible in the display pane.
  • Keep or change the default selections for the parameters.
  • Save the updated report to overwrite the existing version.
Prerequisites
  • The measurement data must be available as historical data logs in the database.
Report inputs
Example:

NOTE: This example only shows selected content from the report, it does not show the entire report.