PME Databases

Power Monitoring Expert uses four databases to store device communication parameters, system configuration settings, and logged historical data.

ION_Network database

Sometimes called the NOM (Network Object Model), the ION_Network database stores device information, such as, device name, device type and connection address (for example, IP address and TCP/IP port or device/Modbus ID). It also contains information about the optional Application Module settings, other ION Servers, Sites, Dial Out Modems, and Connection Schedules. There is only one ION_Network per system.

ION_Data database

The ION_Data database contains the historical data, events and waveforms from devices connected to the system. This includes: onboard logging configured on devices; and, PC-based logging configured in the device translators and the Virtual Processors.

Application Modules database

The Application_Modules database contains configuration settings (for example, layouts, colors, application events, and so on) and cached historical data for some of the Web Applications (for example, Dashboards and Trends).

ION_System log database

The ION_SystemLog database holds system events and their timestamps, which is accessible to view in Management Console. Event priorities can range from 0-255 and are grouped into Diagnostic (0 - 5), Information (6 - 20), Warning (21 - 63), Error (64 - 191), and Critical (192 - 255) categories. System events can include:

  • ION Service stopped or is starting or user connection to an ION Service is lost.
  • Device has been declared offline / online.
  • ION Site Service connected, disconnected or failed to connect to a Site.
  • ION User logs on / off Vista or Designer.
  • ION User saves a Vista or Designer node diagram.
  • Plus many other Warnings and Errors relating to PME system functions.