IP Ports

The following table lists the ports used by PME for the communication between its components and the connected devices:

Port Protocol Location Function Configurable
20/21 FTP Power Meter Power meter access No
23 Telnet Power Meter Power meter access No
25 SMTP Power Meter Power meter access No
69 TFTP Power Meter Power meter access No
80 HTTP (1) PME Server
(2) Power Meter
(1) IIS server, EWS
(2) Power meter access
(1) Yes
(2) No
135 OPC PME Server OPC client No
139/445 NetBIOS/SMB PME Server Engineering client (File and Printer Sharing) No
443 HTTPS (1) PME Server
(2) Power Meter
(1) IIS Server, Cloud Agent
(2) Power meter access
No
502 Modbus TCP Power Meter Power meter communication No
1433 TCP Database Server SQL Server instance No
1434 UDP Database Server SQL Server Browser No
3721 PML Power Meter Power meter communication No
6000-6099 TCP PME Server Log Inserter No
7070 TCP PME Server Licensing Yes
7176 TCP PME Server Diagnostics Viewer (LogSubsystem.Service.exe) No
7700 ION Power Meter Power meter communication No
7701 Modbus RTU Power Meter Power meter communications No
7800 Modbus/ION/PML Gateway Ethergate (All meter COM ports) No
7801 Modbus/ION/PML Gateway Ethergate (Meter COM1) No
7802 Modbus/ION/PML Gateway Ethergate (Meter COM2 and COM 4) No
7803 Modbus/ION/PML Gateway Ethergate (Meter COM3) No
8090 TCP PME Server Web client browser Yes
8523 TCP PME Server Logical devices (LogicalDevice.AutoConfig.ServiceHost.exe) Yes
13666 TCP PME Server PMLNetman.exe No
13667 TCP PME Server Diagnostics Viewer (Server access from client machine) No
13668 TCP PME Server Secondary server No
13666
13670
13671
TCP PME Server Services (Vista and Designer access from client machines) No
23102 TCP PME Server Application Modules web services No
57777 TCP PME Server (1) Real-time data service (to send data to clients)
(2) SQL Server (for default instance)
Yes
57778 TCP PME Server DataProcessorService.exe Yes
57779 TCP PME Server Diagnostics Viewer (Alarm Service) Yes
57780 TCP PME Server Diagnostics Viewer (Log Subsystem) Yes
57781 TCP PME Server Diagnostics Viewer (Cloud Agent) Yes