Alarm to incident mapping

The following table shows the mapping of alarm types to Incidents:

Incident Category Incident Type Alarm Types
Power Quality Interruption Interruption
Over Voltage Over Voltage
Under Voltage Under Voltage
Unclassified Disturbance Unclassified Disturbance
Sag Sag (Voltage)
Swell Swell (Voltage)
Transient Transient
Flicker Flicker
Frequency Variation Frequency Variation
Harmonics Harmonics
Harmonics (Current)
Harmonics (Power)
Harmonics (Voltage)
Unbalance Unbalance
Unbalance (Current)
Unbalance (Voltage)
Diagnostics Communication Status Communication Status
Device Status Device Status
System Status System Status
Energy Management Air Air
Demand Demand
Electricity Electricity
Gas Gas
Power Factor Power Factor
Steam Steam
Water Water
  Asset Monitoring Arc Flash Arc Flash
Backup Power Backup Power
Current Monitor Over Current
Sag (Current)
Swell (Current)
Under Current
Protection Protection
Thermal Monitor Thermal Monitor
General Clutter General Event
Clock / Time
Device Settings
Unassociated Dropout
General Setpoints General Setpoint