Safety Precautions

During installation or use of this software, pay attention to all safety messages that occur in the software and that are included in the documentation. The following safety messages apply to this software in its entirety.

warning

unintended equipment operation

Do not use the software or devices for critical control or protection applications where human or equipment safety relies on the operation of the control action.
Do not use the software to control time-critical functions.
Do not use the software to control remote equipment without proper access control and status feedback.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 

warning

inaccurate data results

Do not incorrectly configure the software or the devices.
Do not base your maintenance or service actions solely on messages and information displayed by the software.
Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.
Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

 

warning

potential compromise of System availability, integrity, and confidentiality

Use cybersecurity best practices to help prevent unauthorized access to the software.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

Work with facility IT System Administrators to ensure that the system adheres to the site-specific cybersecurity policies.