Default ports used for protocols
The following table lists the default ports used for protocols supported by Power Operation. Ports are also customizable.
| Protocol | Port |
|---|---|
| BACnet/IP | UDP/47808 |
| DNP3 | TCP/20000, UDP/20000 |
| Ether Gate | TCP/7801 |
| FTP | TCP/21 |
| HTTP | TCP/80 |
| HTTPS | TCP/443 |
| IEC 60870-5-104 (IEC870IP) | TCP/2404 |
| IEC61850 (MMS) | TCP/102 |
| ION Classic | TCP/7700 |
| ION over TLS | TCP/7443 |
| Modbus TCP | TCP/502 |
| Modbus TCP over TLS | TCP/802 |
| OPC DA | TCP/135 |
| OPC UA | TCP/48031 |
| sFTP | TCP/22 |
| SMTP | TCP/25, TCP/465, TCP/587 |
| SNMP | UDP/161 |
| Telnet | TCP/23 |
| Modbus TCP | TCP/502 |